This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler problem "INTERNAL ERROR: C:\CCStudio_v3.3\C6000 Code Generation Tools 6.1.9\bin\cl6x experienced a segmentation fault while processing"

Other Parts Discussed in Thread: CCSTUDIO

When I use CCS3.3 to compiler a old successful project,I get a error infomation(I install a CCS3.3 and CCS5.2 simultaneously on the computer with Win7 operation system):

INTERNAL ERROR: C:\CCStudio_v3.3\C6000 Code Generation Tools 6.1.9\bin\cl6x experienced a segmentation fault while processing

This is a serious problem.  Please contact Customer
Support with this message and a copy of the input file
and help us to continue to make the tools more robust.

when i uninstall the CCS5.2 and reinstall the CCS3.3,The problom also stands there.

the project can be compilered success on the other computer with WindowsXP operation system,On which I also install a CCS3.3 and CCS5.2 simultaneously .

why?