I've just upgraded from ccsv33 to 40 and I sorely miss the Execution Graph.
There is a webpage "DSP/BIOS Support in CCSv4" "Summary" ( URL =
http://wiki.davincidsp.com/index.php?title=DSP/BIOS_Support_in_CCSv4
) And it shows the following table ...
BIOS 5.2x | BIOS 5.3x | BIOS 5.4x | BIOS 6.xx | |
Build support | Yes | Yes | Yes | Yes |
Runtime Object View | No | No | Yes | Yes |
CPU Load | No | No | Yes | Yes |
Thread Load | No | No | No | Yes |
LOG_Printf | No | No | Yes | Yes |
Execution graph | No | No | No* | Yes |
Statistics Display | No | No | Yes | No |
Notice the "No*" entry. There is not explanation about what the "*" means but it is giving me a glimmer of hope that I might be able to get an Execution graph to work with DSPBIOS 5.4 on CCSV4.
Does anyone have an idea with that "*" means???
Thanks
(P.S. I'll take me answer off line because I'm already late leaving for home)