After replacing my hard-drive and reinstalling CCS3.3 I'm having trouble getting it to connect to my Spectrum Digital XDS510USB probe.
The "emulator test" option in SDConfig reports successful operation, but I have not been able to come up with and combination of settings in the CCS setup that will work.
When I start the CCS setup utility I get an error message:
Error reading one or more XML files: "sdxds510cla.xml" and "sdxds510usbcla.xml"
If I configure CCS as normal to treat my board like a DSK6713 with a Spectrum Digital XDS510USB emulator it can never connect to the probe. The DBGJTAG and XDSPROBE hat I have a target power loss (see below).
Any ideas on how to resolve this issue?
Thanks, Peter Steinberg
C:\CCStudio_v3.3\cc\bin>dbgjtag -f brddat\ccBrd0.dat -rv
-----[Select and reset the controller]---------------------------------------
This utility has selected an XDS510 class product.
This utility will load the adapter 'xds510.dll'.
This utility will operate on port address '0x0'.
That original port address was aliased to '0x0240'.
The controller does not use a programmable FPGA.
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver.
The value is `-180' (0xffffff4c).
The title is: `SC_ERR_CTL_NO_TRG_POWER'.
The explanation is:
The controller has detected a target power loss.