Hi,
I downloaded the full setup for the code composer 5.5 and the inatallation works fine, however when I try to update it I am getting an error and the CC won't start anymore.
I got this problem with 2 pcs already, one with Win7 64 and one with XP.
I believe it is related to the fact that I have a proxy; I have tried to add the proxy settings in the CC before launching the update but still no luck.
The only option is to uninstall it and reinstall it without checking for updates.
Do you have any suggestion? I have attached the installer files as suggested by the error dialog.
Regards,
Marco