This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 5.5 License error after updating



Hi

I have 3 user Floating license. CCS is installed in my system which is also the license server. It was showing as licensed and was working well until now. Today I updated  CGT and xdctools . After that License info is shown as unlicensed. I tried to point to the server location and port , but it gives the following error

I cannot  start the web gui 127.0.0.1:8080 also(as given in http://processors.wiki.ti.com/index.php/License_Server_Administration_for_CCS#Configuring_Code_Composer_Studio

)

I am unable to use the direct license file also.

How can ensure that the server is running?(I have tried disabling the firewall and RT scan)

Thanks

JK