Hello All,
I have been practicing CCS by going through the tutorial provided from help menu
In the topic "Developing A Simple Program", a project \"volume1" is used for explanation. When I follow the steps ,the program builds properly and a .outfile is generated as expected.Let me also mention that in the CCS Setup I am running in F28027(Piccolo) Simulator mode.
Now the problem strikes when i triy to load the program.Loading fails and an error message is generated as follows:
Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
Trouble Writing Memory Block at 0x3f8488 on Page 1 of Length 0x1a: Cannot access memory address 0x3F8488.
The above mentioned memory location ,when I checked out in Piccolo datasheet, is labelled as L0 SARAM.
Here is the linker cmd file for the project:
/****************************************************************************/
/* volume.cmd - Sample linker command file for F28xx devices */
/* */
/* Description: This file is a sample F28xx linker command file that can */
/* be used for linking programs built with the TMS320C2000 */
/* C Compiler. Use it as a guideline; you may want to change */
/* the allocation scheme according to the size of your */
/* program and the memory layout of your target system. */
/****************************************************************************/
-stack 400
-heap 400
MEMORY
{
PAGE 0 : PROG(R) : origin = 0x3E8000, length = 0x10000
PAGE 0 : BOOT(R) : origin = 0x3FF000, length = 0xFC0
PAGE 0 : RESET(R) : origin = 0x3FFFC0, length = 0x2
PAGE 0 : VECTORS(R) : origin = 0x3FFFC2, length = 0x3E
PAGE 1 : M0RAM(RW) : origin = 0x000000, length = 0x400
PAGE 1 : M1RAM(RW) : origin = 0x000400, length = 0x400
PAGE 1 : L0L1RAM(RW) : origin = 0x008000, length = 0x2000
PAGE 1 : H0RAM(RW) : origin = 0x3F8000, length = 0x2000
}
SECTIONS
{
/* 22-bit program sections */
.reset : > RESET, PAGE = 0
.vectors : > VECTORS, PAGE = 0
.pinit : > PROG, PAGE = 0
.cinit : > PROG, PAGE = 0
.text : > PROG, PAGE = 0
/* 16-Bit data sections */
.const : > L0L1RAM, PAGE = 1
.bss : > L0L1RAM, PAGE = 1
.stack : > M1RAM, PAGE = 1
.sysmem : > M0RAM, PAGE = 1
.cio : > M0RAM, PAGE = 1
/* 32-bit data sections */
.ebss : > H0RAM, PAGE = 1
.econst : > H0RAM, PAGE = 1
.esysmem : > H0RAM, PAGE = 1
}
Please help as to what changes need to be made.
Thanks in advance
Regards,
J D