Here's another new user question:
Per SPRAAT2F,
The C6748/C6746/C6742 bootloader has undergone multiple revisions. To check the version of your
device, perform the following steps.
1. Connect to the device in the Code Composer Studio™ software.
2. Select View → Memory.
3. Enter the address of the beginning of the ROM, 0x11700000, at the top of the memory window.
4. Select Character mode at the bottom.
The text d800k008 should appear in the memory window at offset 0x08.
Allright. How do I select character mode, presumably at the bottom at the bottom of the memory window?