This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Debugging two devices simultaneously

Hello,

I have a TMDSEVM6657LS and a TMDSEVM6657LE. The LS variant uses a XDS200, and the LE uses a XDS560v2.

I'd like to debug both of these cards at the same time using code composer. Currently, I can debug each of them independently without any issues.

To do this, I created a new Target Configuration File. I've attached this file. I had to renamed it to a .xml file because of the forum software.

When I use this target configuration, I get the following error:

C66xx_0: GEL Output: Setup_Memory_Map...
C66xx_0: GEL Output: Setup_Memory_Map... Done.
IcePick_D: Error initializing emulator: (Error -2083 @ 0x0) Unable to communicate with the emulator. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.1.232.0)

Does anyone have any ideas on how to fix this issue?

Additional Information:

  • Code Composer Version: 5.5.0.00077
  • Windows Version: 8.1