This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The status of standalone simulator load6x

Hi!

There is a standalone simulator provided with the Linux version of CGT for C6000 called load6x (load6xexe to be correct). As far as I understand it simulates C6201 core and requires pretty old version of shared C++ runtime which is not available in the recent distors. Moreover, this tool tends to coredump on certain distors with unknown reason. Is this tool being developed or it is discontinued? Will it support recent kernels (C64x or C64x+) in the near future?


Thanks, Max