Other Parts Discussed in Thread: OMAP5912
Running CCS 3.3.82.13, when I try to run the CPU Load Graph by choosing CPU Load Graph from the DSP/BIOS menu, I get an error message dialog: title bar: CPULOA~1; message text: An unsupported operation was attempted.
In the past this feature has worked for me. I'm not sure at what point it quit working. I suspect it may be related to the most recent version of CCS. Other DSP/BIOS diagnostic features still work (Execution Graph, Message Log, Kernal/Object View).
The other thing that is interesting is that I get the exact same error dialog if I try to run the CPU Load Graph before I have a program loaded on my target, and before I have a project loaded, i.e. immediately after connecting to the target. This makes it seem like it's some kind of a conflict on the PC in being able to run software to support the CPU Load Graph - perhaps a plugin or some such.
I am connecting to a C55 core in an OMAP5912, via an XDS510 USB. I am running DSP/BIOS 5.31.08. I am using Code Generation Tools v3.3.6.