This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Inconsistent relative include paths in CCS3.3



We want to use an option file in our project to generate a common "include path" for debug & release version.

We stumpled upon the following problem:

  • We know, that $(proj_dir) is not allowed in the options file [:(]
  • When using relative paths the include path must be relative to the source file - Ok, that would be fine for us
  • When using program level optimization "-pm -op2", the relative path is not anymore relative to the source file (may be relative to $(proj_dir) or some temporary file)

So we are unable to use the same options file for debug & release version.

Is this a known problem and does anyone has a solution for it?

 

Thanks

Jan