Hi,
I have downloaded the program sprc207 for Implementation of sensored Indirect FOC of Induction motor for TMS320F2808. It was written for ccsv3.3.
But I'm using ccs Version: 5.5.0.00077. On building aci3_3.pjt using the 'Import legacy 3.3 projects' option i get the following linker error as given below.
>> Compilation failure
_DLOG_4CH_init C:/tidcs/DMC/c28/v32x/sys/ACI3_3_280x/cIQmath/obj/aci3_3.obj
_DLOG_4CH_update C:/tidcs/DMC/c28/v32x/sys/ACI3_3_280x/cIQmath/obj/aci3_3.obj
_F280X_CAP_Init C:/tidcs/DMC/c28/v32x/sys/ACI3_3_280x/cIQmath/obj/aci3_3.obj
_F280X_CAP_Read C:/tidcs/DMC/c28/v32x/sys/ACI3_3_280x/cIQmath/obj/aci3_3.obj
_F280X_DRIVE_Init C:/tidcs/DMC/c28/v32x/sys/ACI3_3_280x/cIQmath/obj/aci3_3.obj
_F280X_DRIVE_Update C:/tidcs/DMC/c28/v32x/sys/ACI3_3_280x/cIQmath/obj/aci3_3.obj
_F280X_PWMDAC_Init C:/tidcs/DMC/c28/v32x/sys/ACI3_3_280x/cIQmath/obj/aci3_3.obj
_F280X_PWMDAC_Update C:/tidcs/DMC/c28/v32x/sys/ACI3_3_280x/cIQmath/obj/aci3_3.obj
_F280X_PWM_Init C:/tidcs/DMC/c28/v32x/sys/ACI3_3_280x/cIQmath/obj/aci3_3.obj
_F280X_PWM_Update C:/tidcs/DMC/c28/v32x/sys/ACI3_3_280x/cIQmath/obj/aci3_3.obj
_F280X_ileg2_dcbus_drv_init C:/tidcs/DMC/c28/v32x/sys/ACI3_3_280x/cIQmath/obj/aci3_3.obj
_F280X_ileg2_dcbus_drv_read C:/tidcs/DMC/c28/v32x/sys/ACI3_3_280x/cIQmath/obj/aci3_3.obj
_clarke_calc C:/tidcs/DMC/c28/v32x/sys/ACI3_3_280x/cIQmath/obj/aci3_3.obj
_ipark_calc C:/tidcs/DMC/c28/v32x/sys/ACI3_3_280x/cIQmath/obj/aci3_3.obj
_park_calc C:/tidcs/DMC/c28/v32x/sys/ACI3_3_280x/cIQmath/obj/aci3_3.obj
_pid_reg3_calc C:/tidcs/DMC/c28/v32x/sys/ACI3_3_280x/cIQmath/obj/aci3_3.obj
_rampgen_calc C:/tidcs/DMC/c28/v32x/sys/ACI3_3_280x/cIQmath/obj/aci3_3.obj
_rmp_cntl_calc C:/tidcs/DMC/c28/v32x/sys/ACI3_3_280x/cIQmath/obj/aci3_3.obj
_speed_prd_calc C:/tidcs/DMC/c28/v32x/sys/ACI3_3_280x/cIQmath/obj/aci3_3.obj
_svgendq_calc C:/tidcs/DMC/c28/v32x/sys/ACI3_3_280x/cIQmath/obj/aci3_3.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "../aci3_3.out" not built
gmake: *** [../aci3_3.out] Error 1
gmake: Target `all' not remade because of errors.
How can I resolve the errors?