Other Parts Discussed in Thread: TMS320F28335
Hi together,
- I have CCS 4.0.2.01003
- I use the TI Example (Example_28335 Flash) and adapt it to a Serial I/O functionally, but I keep the memory map and the password.asm file exact the same one like in the example
- I use the TI Peripheral Explorer with a tms320f28335 - The JTAG adapter is C2000 510LC USB JTAG Device, flash voltage is 5V (Jumper is set on the board) after unpacking the example kit and flashing/debugging the project, a flashing error message comes and the first flash fault…
The following flash messages come at the next desperate bid to connect to the target: C28xx:
"Flash Programmer: Device is locked or not connected. Operation cancelled. C28xx: Trouble Writing Memory Block at 0x3389b2 on Page 0 of Length 0x1f Cannot write to target "
I have no Idea, because this ist the second DIM module that comes fresh from the box and brings this message in the flash console window. the Flash OSCCLK is 20 Mhz, the CLKINDV is 2 and the PLL Value is 10. can you help me to fix the problem? Regards Heiko