This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS V5.5 ARM Compiler 5.1.1 update failure



Hello,

I am working with CCS V5.5 and ARM compiler 5.1.1.  I am using a couple of the TIVA M4 parts.  In order to gain uniforminty within the company, I was attempting to update my compiler to 5.1.2 through CCS.  Using help->install new software, I was able to  find ARM compiler tools version 5.1.2.  I installed and CCS requested I restart CCS for the changes to be implemented.  When CCS reboots, a "Code Composer Studio V5 Setup" install icon apears on my desktop and the install just hangs there.  No progress.  If I close the icon and launch code composer the same icon appears and hangs. 

 

This is a company machine running windows 7.  There is anti virus software that I can not disable.  Has anyone else had this error?  What else can I be looking at?  This is my second attempt at updating the ARM compiler.  I had to do a fresh install of CCS (which is a real pain) in order for CCS to launch again. 

 

Any help would be greatly appreciated!

 

Jeff