This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Spectrum Digital XDS560v2 PRO TRACE Receiver trace too slow



hello:

I have bought a XSD560V2 PRO trace emulator from TI estore, I use it to trace data from c6678 EVM. I set the buffer size to 128MB and 10 pin in the receiver/transport settings, when my application run few seconds, the buffer is full and then stop, here it need about 4 hours to get the trace data from the trace box buffer to update onto the CCS5.5.

Yes if I set the buffer size to 1MB, it will several minutes, but it does not meet my need, if I set the buffer to 1GB, it will  spend many time to trace the data out.

So I want to know whether there is anyway to short the trace time. Thanks.

Best Regars,

Si