I am using CCS 4.0.1.01001, Code Gen 6.1.9, BIOS 6.20.1.41. I am using a copy of the unlicensed tools that I downloaded last week.
I created a project based on the Clock Example template using the RTSC Target ti.targets.C64P and RTSC Platform ti.platforms.sim64Pxx. When I run the debugger nothing is ever printed to the console. If I stop the debugger it is usually in the Idle loop.
I have created projects based on the Hello Example template and Error Example template and they work.