Hi
I am using CCS Version: 5.5.0.00077.
I have an older project that was built using TI compiler 4.9.1.
I have changed the compiler version to 5.1.1 within CCS.
However, the subdir_rules.mk file still has 4.9.1 path in it. This can be seen when I try to build clean. NB. subdir_rules.mk is rebuilt each time.
Please can someone advise how to convince CCS to create the subdir_rules.mk file containing the reference to 5.1.1.
Thanks
Part of subdir_rules.mk
BMS_OS.obj: ../BMS_OS.c $(GEN_OPTS) $(GEN_SRCS)
@echo 'Building file: $<'
@echo 'Invoking: ARM Compiler'
"C:/ti/ccsv5/tools/compiler/tms470_4.9.1/bin/cl470" -mv7R4 --code_state=32 --float_support=VFPv3D16 --abi=eabi -g --include_path="C:/ti/ccsv5/tools/compiler/tms470_4.9.1/include" --gcc --diag_warning=225 --display_error_number --enum_type=packed --preproc_with_compile --preproc_dependency="BMS_OS.pp" $(GEN_OPTS__FLAG) "$<"
@echo 'Finished building: $<'
@echo ' '
Build Log
**** Build of configuration Debug for project BMS OS ****
"C:\\ti\\ccsv5\\utils\\bin\\gmake" all
'Building file: ../BMS_OS.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv5/tools/compiler/tms470_4.9.1/bin/cl470" -mv7R4 --code_state=32 --float_support=VFPv3D16 --abi=eabi -g --include_path="C:/ti/ccsv5/tools/compiler/tms470_4.9.1/include" --gcc --diag_warning=225 --display_error_number --enum_type=packed --preproc_with_compile --preproc_dependency="BMS_OS.pp" "../BMS_OS.c"
The system cannot find the path specified.
gmake: *** [BMS_OS.obj] Error 1
**** Build Finished ****