Support,
This is an enhancement request. Is it possible to change the way CCSv4 handles the situation when one tries to import a project with the same name as a project that already exists in the workspace? In v4.1 the import wizard just omits the project names from the available projects at the selected root directory. It would be better if the project were shown but greyed out and with a note saying something like "project already exists in current workspace". I have seen new users waste time with this when following instructions for importing example projects. They don't realize the project is already added to their workspace and they keep trying to check the import path.
Ruben