This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ,
i need you help, i got a new kit , after - Click Project “Rebuild All” , I need to ”Debug Active Project”. then i got error :
C28xx: Flash Programmer: Error erasing Flash memory.
C28xx: Flash Programmer: Error encountered when writing to flash memory
C28xx: Trouble Writing Memory Block at 0x3f6000 on Page 0 of Length 0x1839
Cannot write to target
can you pls help me I tried to earse and strat over but still no success what shoul I do ?
Hi,
Have you set the target configurations correctly? Also, are you importing the example codes or are they custom ones?
Regards,
Gautam
thanks for the quick repaly ,
yes i set the target configurations correct and import example code , the build is seucss but the Debug Active Project is failed;
C28xx: Flash Programmer: Error encountered when writing to flash memory
C28xx: Trouble Writing Memory Block at 0x3f6000 on Page 0 of Length 0x1839
Cannot write to target
yotam
Yotam, I hope your MCU is not in a locked condition. What you can check is download CCS Uniflash and use the unlock feature in it and then try programming using the same application. Let me know what you observe.
Regards,
Gautam
Gautam Hi,
thank you for anwsring yesterday i try to flash the memory card with uniflash but the program (uniflash) and now also the programming cc4 are now telling me the the chip is TMS320F28027 when the chip on the bord is TMS320F28035. The erorr messge is: canot find the device ...35 the dedcted device is ...27.
can you pls try to help me as soon as possible .
Yotam
Yotam, I somehow feel your device has been permanently locked. Check this link for more info:
http://e2e.ti.com/support/microcontrollers/c2000/f/171/t/115770.aspx
Regards,
Gautam
gautam Hi ,
after debaging i get this messge :
C28xx: Flash Programmer: Warning: The configured device (TMS320F28035), does not match the detected device (TMS320F28027). Flash Programming operations could be affected. Please consider modifying your target configuration file.
C28xx: Flash Programmer: Error erasing Flash memory.
pls try to help
yotam