I am attempting to make a software mod to a 3 year old product based on the MSP430. The original developers (hardware and software) have left the company. The original development was done on an old machine with a single user license using CCS3. Since there are 3 of us left here in the group who might make software tweaks to the device we decided to spend the money to get a single user floating license version of CCS5. CCS5 is installed and working fine ( Version: 5.5.0.00077 ) on my PC (Windows 7 Pro SP1 64-bit). After making the changes I hooked up the MSP-FET430UIF emulator, and attempted to debug. CCS noted that the firmware on the emulator needed to be upgraded, and I followed the directions for the upgrade. After upgrading I get an error indicating that the device is unknown.
After perusing these forums I have attempted to use the IAR compiler instead which changed the FET firmware revision also, but also failed to detect the device. I downloaded FET-Pro430-Lite which also wanted to update the firmware, and also failed to communicate with the device.
Finally I found a post on this forum by Lisa - TI which said CC5 wasn't intended for use with MSPs, and that a downgrade to V2 on the FET could fix the problem. Granted, that user had downgraded to CC4 from CC5 when he had the problem. In any case all I've proven is that V2 isn't compatible with CC5, and that CC5 will attempt to upgrade the firmware before debugging.
This was a working unit prior to connecting the FET to the JTAG interface and attempting to debug, so I don't believe the processor is damaged. The voltage is 3.0 volts.
I have seen enough chatter online to believe it's some sort of compatibility issue between the FET, CC5, etc., but can't find a definitive answer anywhere that says to use a particular version of CC5, msp430.dll, and FET firmware.
Any suggestions?