Hi,
I have a RTSC project running on a LM3S9D96 platform. The project was an existing project that I have had no problems with in CCS 5.5. Now when you debug the project it programs the FLASH and will sit indefinitely without launching the debugger. If I remove the "run to main" the code runs fine but the debugger will not launch. Yet. Another Similar Project will run on the same platform with the same debugger. I cannot see any differences between the configurations, its very strange. Is there any logging or verbose mode that will help resolve this problem?
Thanks.