This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Complex LCF with UNION's and copy TABLE's

Hi,
I try to write a application where I have to copy three different algorithms in the RAM, to safe RAM I like to use UNION's to allocate the RAM three times.

Each algo consists out of different functions, one function will be used in two algos.

I wrote the following LCF, which works:

    UNION : run=RAM
    {
        GROUP : table(__SetActiveBank_Table), load=FLASH0
        {
            .text:Fapi_setActiveFlashBank      : {} palign=8
            .text:_scaleEEFclk                 : {} palign=8
            .text:_scaleMainFclk               : {} palign=8
        }

        GROUP :
        {
            UNION :
            {
                GROUP : load=FLASH0, table(__ProgrammFlash_Table)
                {
                    .flashBytesWithEcc                 : {} palign=8
                    .text:Fapi_issueProgrammingCommand : {} palign=8
                    .text:Fapi_calculateEcc            : {} palign=8
                }

                GROUP : table(__EraseSector_Table), load=FLASH0
                {
                    .flashEraseSector                       : {} palign=8
                    .text:Fapi_issueAsyncCommandWithAddress : {} palign=8
                }
            }

            .text:_Fapi_issueFsmCommand        : {} palign=8, load=FLASH0, table(__issueFsmCommand_Table)
        }
    }


Then I tried to get rid of the copy TABLE(__issueFsmCommand_) and replaced it by table(__ProgrammFlash_Table), table(__EraseSector_Table).

Now the Linker gives me the following warnings:

"../sys_link.cmd", line 96: warning #10110-D: table(__EraseSector_Table)
   operator ignored:  table(__EraseSector_Table) has already been applied to a
   section in the UNION "UNION_1" in which ".text:_Fapi_issueFsmCommand" is a
   descendant
"../sys_link.cmd", line 96: warning #10110-D: table(__ProgrammFlash_Table)
   operator ignored:  table(__ProgrammFlash_Table) has already been applied to
   a section in the UNION "UNION_1" in which ".text:_Fapi_issueFsmCommand" is a
   descendant

And the resulting tables don't contain: .text:_Fapi_issueFsmCommand

Combining these would help to make the application less complex as it would save some calls of copy_in().

Is there a reason why I can't combine a GROUP member and UNION members in one COPY table, or is this a bug?

Thanks,
Christian

  • Every member of a UNION must have a separate copy table.  The linker does not support somehow combining copy tables together.

    Thanks and regards,

    -George

  • I took a look at this test case and I think it's a reasonable use case.  However, it's not a bug, because the linker works as designed.  I've submitted SDSCM00050128 as an enhancement request to add this feature.

    Abbreviated, the user wants to do this:

        UNION("outer")
        {
            GROUP
            {
            }
    
            GROUP("X")
            {
                UNION
                {
                    GROUP : table(tableB)
                    {
                    }
    
                    GROUP : table(tableC)
                    {
                    }
                }
    
                .something: table(tableB), table(tableC)
            }
        }
    

    It doesn't matter that tableB and tableC are re-used under UNION("outer"), because GROUP("X") ensures that they cannot overlap.

  • Thanks for looking into this.

    As of today none of my customers is requesting this feature, but I would wonder if nobody else has or would like to do this type of function overlapping.

    Best Regards,
    Christian

  • It's not extremely surprising this issue hasn't come up before.  It requires both nested overlays and re-used table names; the overhead for keeping separate tables is relatively small, so the workaround is feasible.

  • Hi,

    I verified the changed behavior with the TI ARM CGT 5.1.6 and 5.2.0A14136, both linker versions are now able to handle my use case correctly.

    Thanks,
    Christian

  • That should not be possible.  The enhancement was only added to the 5.2.0A branch, not the 5.1.x branch.  Are you positive you were using 5.1.6 when you tested it?

  • Yes, I'm sure.
    I was also a little bit surprised that this now works with 5.1.6.

    Here is the extract from the MAP file:

    ******************************************************************************
                      TI ARM Linker PC v5.1.6                      
    ******************************************************************************
    >> Linked Tue May 20 08:28:55 2014

    ...

    __ProgrammFlash_Table @ 00008cb0 records: 4, size/record: 12, table size: 52
        .flashBytesWithEcc: load addr=00000020, load size=00000100, run addr=080016a0, run size=00000100, compression=none
        .text:Fapi_issueProgrammingCommand: load addr=00000120, load size=00000168, run addr=080017a0, run size=00000168, compression=none
        .text:Fapi_calculateEcc: load addr=00000288, load size=00000018, run addr=08001908, run size=00000018, compression=none
        .text:_Fapi_issueFsmCommand: load addr=000004e0, load size=00000040, run addr=080019c0, run size=00000040, compression=none

    __EraseSector_Table @ 00008ce4 records: 3, size/record: 12, table size: 40
        .flashEraseSector: load addr=00000440, load size=00000070, run addr=08001920, run size=00000070, compression=none
        .text:Fapi_issueAsyncCommandWithAddress: load addr=000004b0, load size=00000030, run addr=08001990, run size=00000030, compression=none
        .text:_Fapi_issueFsmCommand: load addr=000004e0, load size=00000040, run addr=080019c0, run size=00000040, compression=none


    Best Regards,
    Christian