We have two PC's with Windows2000 and Code Composer Studio V3.3 installed.
The Versions are as follows:
- Windows 2000 SP4, 5.00.2195
- CCS V3.3 Platinum, V3.3.82.13
Until 24.09.2009 CCS V3.3 worked fine. But when we had to use it last Friday (05.02.2010) CCS V3.3 crashed shortly after the splash screen appeared with the following message:
The Visual Studio shows the following message:
There was a similar post addressing probably the same problem. There they ask to rename "cwsense.dll". I have done this but without success.
We did not make any changes to CCS V3.3. I have also tried to uninstall and install again. First without SR12 (--> same problem) and then with SR12. In vaine so far.
Attached is a dump file from CCS V3.3.
Any ideas what happend?