Other Parts Discussed in Thread: OMAPL138
Hey Champs,
I want to run an IPC example on the OMAPL138 in CCS4.1 by using the XDS510USB emulator. For this purpose I have to run an application on both cores, C674x and ARM9. For the DSP everything is working fine.
However on the ARM side I can only connect and download the out-file. Afterwards I the core seems to run automatically and can't be reset or re-started. Also the program never reaches the main function. The dis-assembly view shows no data and when I pause the program the PC is pointing to a reserved memory area (0x00DC49A45):
I already tried out several different target configuration settings like OMAPL138 or EVMOMAPL137 and included the gel files from the Logic PD homepage.
Could you please advise on what's going wrong here?
Thanks and best regards, Christoph S.