This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can't create SYS/BIOS project after CCS5.5 reinstall

Other Parts Discussed in Thread: OMAPL138, OMAP-L138

Hi!

For some reason I corrupted my installation yesterday (CCS5.5 and MCSDK, working with SYS/BIOS 6 on the DSP of the OMAPL138 LCDK on Win7).

Today I reinstalled
CCS5.5;
CodeGen tools;
MCSDK1.1

and I wanted to get the environment running again.

Unfortunately I can not setup a SYS/BIOS project any more because in the
RTSC Configuration Settings dialog the Target-line is empty.

Also the available options for various targets are missing  in the IT Resource Explorer window:

In my old installation there were entries for the LCDK L138 and many more.

During the installation there was (as far as I remember) no option for multicore/C6000 DSP that I unchecked.

Running the ccs5.5 setup again, I see what I checked during installation:

Afaik the OMAP-L138 should be installed on my system.

Can anyone help me with a suggestion what went wrong?

Thanks a lot,

Alexander