This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does the simulator support configuration of FSYNC model?

Hi,

     Whenever I run the simulator, the following messages come out,

Default constructor for frame_sync_intf_t called

Constructor for FSync model called

Initializing FSync model

time0: 0 : reset

aif_parms_init2 - finished reading the scenario files

Initializing FSync model

System.FARADAY.SHARED_SYSTEM.USER5 : AI Reset interface - start

time0: 0 : reset

aif_parms_init2 - finished reading the scenario files

Illegal value for addr_10_13 = 0

 

It seems that FSYNC model can be configured by the simulator, doesn't it? How could I configure the FSYNC model in simulation environment?

 

Br,

AppleCat