I'd like to use TMDSCCS-ALLN01 to my RDK-IDM-L35 - Stellaris board, but
I don’t know can I download ccs v.4 or v.5 on trial 30 day time.
Can somebody help me?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'd like to use TMDSCCS-ALLN01 to my RDK-IDM-L35 - Stellaris board, but
I don’t know can I download ccs v.4 or v.5 on trial 30 day time.
Can somebody help me?
Hi Andrzej
I am not sure what you are asking? Do you have a license? Are you asking where to get a demo?
CCS is here, a demo of the latest version would be v6.
http://processors.wiki.ti.com/index.php/Download_CCS
If you are asking what type of license you purchased ... the license team can help
Best Regards,
Lisa
From Your forum of TI:
“Hi,
I am using RDK-IDM-L35 with 90day free evaluation licence of CCS v4.1.1. When I attempt to connect to L35 i have got "invalid licence" message so i can not connect to L35.
Is this problem related to free evaluation licence or not? If not, is there any fix for that problem?
Thanks.. “
I think that for RDK-IDM-L35 – Stellaris the better will be CCS v4.1.1. but CCS v5 or v5 will not be good.
The best regards.
Andrzej M.
I think that for RDK-IDM-L35 – Stellaris the better will be CCS v4.1.1. but CCS v5 or v6 will not be good.
The best regards.
Andrzej M.
Hi,
I have RDK-IDM-L35 - Stellaris and JTAG EMULATOR, 20/10PIN, XDS100 v2 Blackhawk CCS v5 Now I bought the new one ccsv6 Activation ID : 5B55-37D0-ED8D-11E3-85C4-C3B3-1ABA-B367.
When I worked with ccsV5 , I could open every examples from my CD-ROM.
Now when I bought the new one ccsv6 i can open only first Hello World example, but others do not want open.
After debug session on the screen apears white flash and after moment the screen is black.
When I step program in debuger by "Run to line " display show only first widget ( lang demo, grlibdemo,hellowidget)
but it stops on the TouchScreenInit(); After this appears message:
CORTEX_M3_0: Can't Run Target CPU: (Error -1268 @ 0x90001) Device is locked up in Hard Fault or in NMI. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.450.0)
Debuger windows shows message: _c_int00() at boot.asm:217 0x0000ABAE (_c_int00 does not contain frame information) in every step.
What can I do this the ccsv6 works like ccsv5?
The best regards.
Andrzej M.