Other Parts Discussed in Thread: CCSTUDIO, TMS320C6455
Hi,
I've got a DSK6455 and I've been using CCSv3.2 as installed from the DSK CD.
I want to use CCSv4 because I've no real investment in CCSv3 so going to the newest version seems obvious.
Unfortunately I can't to the DSK using CCSv4. I guess this is a SD emulator problem but I hoping someone on this forum will be able to help me out!
Here's what I've done so far:
- Read the SD installation notes (http://support.spectrumdigital.com/ccs40/) which say install CCSv4
- Downloaded and installed CCS V4.0.1 (Platinum)
- Connected the DSK and told the driver install dialog to look in C:\Program Files\SpectrumDigital\Emulation\Drivers\i386
- Driver install appeared to go okay
- Noted that there was no "Setup CCStudio v4.0" desktop or start menu icon as mentioned in SD guide
- Ran CCSv4 and selected File|New|Target Configuration File
- I wasn't sure what to select from the Connection list but selected SD DSK-EVM-eXdsk onboard USB emulator because that allowed me to check DSK6455
- Clicked Save
- Returned to the project and tried to debug
- Clicked Unblock when some security message about JavaVM appeared
- Got various emulator/connection errors, cancelled all the errors
- Ran SdConfigEx v4 from desktop icon
- SdConfigEx v4 shows XDS510USB at 510, 511, 512 & 513.
- Verfify Connection gives "XDS510-USB Emulator not connected/enumerated" for any of these
- Couldn't see anything worth changing in SdConfigEx
- Ran DSK6455 Diagnostic Utility v3.2
- Noted that it said "Emulator Address :0x540"
- Spent some time messing around with connection types, SD notes, etc
Any hints, suggestions or thoughts greatly appreciated!
Thanks,
Matt