This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C Run-time reentrancy function list for various DSP platforms?



Looking through the help for the 2407a and the F28335 C compiler help, I am unabled to determine which (if any) functions are advertised as being reentrant?

While I am aware of the usual suspects like strtok, printf, malloc, etc, on any platform, I am wondering if there is a master list somewhere?

Here is a snippet I found in the help about eXpress complient algorithms, it is the only section in the help that I could find that addresses the issue.

Thank you.

---

The following table summarizes the TI C-Language Run-time Support Library functions that may be referenced by eXpressDSP-compliant algorithms.

Allowed or disallowed  Category  Typical functions in category  Notes
allowed  String functions  strcpy, strchr, …  1
allowed  Memory-moving functions memcpy, memmove, memset, ...  2
allowed  Integer math support  _divi, _divu, _remi, _remu, ... 2
allowed  Floating point support  _addf, _subf, _mpyf, _divf, _addd, _subd, _mpyd, _divd, log10, cosh, ... 2, 3
allowed  Conversion functions  atoi, ftoi, itof, ...  2
disallowed  Heap management functions malloc, free, realloc, alloc, …  5
disallowed  I/O functions  printf, open, read, write, …  4
disallowed  misc. non-reentrant functions printf, sprintf, ctime, ...  5, 6
Notes:

1)  Exceptions: strtok is not reentrant, and strdup allocates memory with malloc.
2)  Some of these are issued by the compiler automatically for certain C operators.
3)  The errno paradigm isn't reentrant. Thus, errno must not be used by eXpressDSP-compliant algorithms.
4)  Algorithms are not allowed to perform I/O (except via DSP/BIOS APIs).
5)  Algorithms must not allocate memory.
6)  Algorithms must be reentrant and must, therefore, only reference reentrant functions.