Hi all,
I am using CCS Version 4.1.0.02006 to which I am migrating a CCS 2.20 project (creating a new project, not importing).
When building, the compiler complains that the following files cannot be found:
csl.h, csl_xbus.h, csl_irq.h
I thought I would have to add an include path but these files do not exist in the TI directory at all! When installing I selected "C6000 DSPs" only but every box after that was selected.
Has there been a paradigm shift from 2.20 to 4.xx meaning some significant porting is required now for the code or is this (hopefully) something much simpler?
Many thanks,
Ken