This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Autoscale problem still there in CCSv6.0

It has been a very annoying issue in CCS5.x that the autoscaling of graph display does not work.

Seems this issue is still there in CCS 6.0.

It was working well in legacy CCS v3.3...

  • Hello,

    There was a fix to address this. It should be in version 5.5 and 6.0. Can you describe the exact issue you see? Note that the autoscale only happens for higher values.

    Thanks

    ki

  • Thank you ki.

    I sample an ADC value periodically (40kHz) and put it into an array. Then open a graph window to watch the array. It was basically a sine wave. But the plot cannot autoscale to the wave, I have to zoom vertically by hand. I tried clicking "Refresh", "Reset Autoscale" and "Auto Scale" options but there was no effect.

    I know when the values are too small (say all the way zero) the autoscale does not work. But my value is -1000 to +1000 and I can watch it by manual zooming. However autoscale seldom triggers (yes it works occasionally...)

    Could you tell me where to find the fix? I know there was a fix for CCS5.4 after searching the forum, but I cannot find one for CCS 6.0.