Other Parts Discussed in Thread: CCSTUDIO, TMS320F28035
The CCS Team has released a patch to CCS 4.0 to improve stability and performance of Flash Programming on F28x devices. This patch is recommended for all C2000 users. The patch is 250kB in size and will download and install quickly.
CCS 4.1 users should ensure they have version 4.1.0.2006 or later. Also note that CCS version 4.1.1 is expected to be released prior to Feb 24, so developers upgrading from 4.0 to CCS 4.1 are recommended to wait for the release of 4.1.1 to minimize download and installation times. There will be an update available through update manager that will update all prior CCS 4.x releases to 4.1.1. The update will be made available shortly after the posting of the 4.1.1 full install.
For more information, please refer to the Release notes:
Installation
The update is installed via the Eclipse update manager. Select “Help -> Software Updates -> Find and Install …”, then “Search for updates of the currently installed features”. When the list of available updates is displayed, select the 4.0.4.01000 update and allow it to be installed.
This update is only applicable to CCS 4.0.2. If you have a different version of CCS, you will need up update to 4.0.2 first.
Content
Some customers have reported that Flash speeds for C28 are slower than expected. A small number of customers have also reported issues with locking devices. The slower than expected flashing speeds are due to an error in the clock frequency calculations for C28x devices. The update addresses this C28 specific problem.
http://software-dl.ti.com/dsps/dsps_public_sw/sdo_ccstudio/CCSv4/CCS_4_0_4/ReleaseNote.htm
Please post any questions, problems or general feedback regarding the patch in the Code Composer Studio forum.