Other Parts Discussed in Thread: CCSTUDIO
Good day experts,
I recently upgraded to CCS 5.5 from CCS 5.4 and I am experiencing annoying crashes while in the debug perspective.
My setup is as follows:
- Win 7 64-bit
- CCS v5.5.0.00077
- Target: C6748 DSP running a DSP/BIOS 5.42.01.09 based application
- Emulator: Spectrum Digital XDS560v2 STM
When I am in the debug perspective of CCS, I display the CPU load graph from the Tools -> RTOS Analyzer -> RTA (Legacy) menu. The CPU load is displayed correctly for about 5 minutes while the application is executing and then CCS just closes (crashes) without displaying any message. I have attached the log file of my workspace.
What I have tried so far, based on similar posts (but did not work):
- Renamed ctools.dll to ctools.bak in ti\ccsv5\ccs_base\emulation\analysis\bin
- I never had a CCS 3.3 installation on my PC, so there are no apparent incorrect paths in my PATH environmental variable.
Can you please assist as this is extremely annoying!