Hi,
Tried to install CCS 5.5 on XP SP3, but it failed. I've attached the installation log.
Any help would be GREATLY appreciated!
1512.ccs_setup_5.5.0.00077_install.log
Shian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Tried to install CCS 5.5 on XP SP3, but it failed. I've attached the installation log.
Any help would be GREATLY appreciated!
1512.ccs_setup_5.5.0.00077_install.log
Shian
Hi Shian,
Eclipse is unable to handle non-ascii characters in the temporary directory which is created using the username.
Please create a temporary user with admin privileges with an ascii user name. Install for all users, as administrator. Please make sure the install directory is empty.
You will then be able to run CCS as yourself.
Danish