This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS full and Piccolo CLA support?

Hi all,

I am currently using CCS 3.3 SR13 (3.3.82.13) full with Piccolo 28035 and would like to have full CLA support.

Update advisor only links to the 32k-limited CCS version, but I don't want to install a second CCS.

Switching to CCS4.0 is no option since it does not support CLA at all.

After installing the chip support package, I get some Piccolo support, but not all.

I can't set breakpoints or single step through CLA code, although the MDEBUGSTOP command ist present in the code.

So how do I get full CLA support without 32k-limit?