|
hello.... when i connect msp430g2 launchpad to the usb port,showing the warning that the "device driver is not installed successfully " and device manager showing Device status: "The drivers for this device are not installed. (Code 28)", in CCS when i attempted to launch the project the console shows "MSP430: Error initializing emulator: No USB FET was found" i tried to install the driver manually using device manager but windows says that it cant find the driver.... please help me to get rid of this problem....... |