Hi Forum
I have had CCS6 crashing the computer 6 times yesterday and causing the BSoD. It happens particularly when I try to run the debugger. Please see the report below:
Problem signature:
Problem Event Name: BlueScreen
OS Version: 6.1.7601.2.1.0.256.1
Locale ID: 1033
Additional information about the problem:
BCCode: 3b
BCP1: 00000000C0000005
BCP2: FFFFF8000368C1A4
BCP3: FFFFF8800BE7BDF0
BCP4: 0000000000000000
OS Version: 6_1_7601
Service Pack: 1_0
Product: 256_1
Files that help describe the problem:
C:\Windows\Minidump\060914-23743-01.dmp
C:\Users\windows7\AppData\Local\Temp\WER-50622-0.sysdata.xml
I have got a screen shot of the BSoD. Also I can send the above two files. I am running the SD Traveler debugger.
Previously I have been able to run without a problem but I think this started happening with the recent updated from TI for the SD emulators. Has anyone experienced the above problems?
Thanks
Manjula
Has anyone