This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CLA debuggin issue in CCS4.1

Hello!

I'm trying to debug a project using CLA in CCS4.

I found a problem in register watch window when using float data.

I tried placing a float (0.05) in memory, read and write back.

If I see memory and watch as float it is 0.05 in hex 0x3D4CCCCD.

In register watch I see it as 0x3D4CCCCD hex (correct) but is shown as 1.028443341e+09 (WRONG!) in float.

I tried adding +20000 or multiplying for 2 that value, result stored in RAM are correct (shown in float) but when I see them from register view it is wrong 1.184628761e+09 and 1.036831949e+09

Some ideas?

Loriano

p.s Code Composer Studio  Version: 4.1.0.02003 ; System is Window XP SP Pro 2002 SP3; target is a Piccolo Experimenter's Kit 28035, XDS100 V2 USB emulator. Project is run in FLASH .