I downloaded the file TI_CGT_C6000_6.1.10_setup.exe from the TI update web site. I did not get any errors and the file appears to be intact. However, when I try to run this file either from Windows Explorer or from a CMD window it immediately returns to the command prompt and nothing happens. I don't see any errors or anything. This is some problem with my OS I think but I can't figure out what could cause this. Has anyone else heard of something like this?
Dan