This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
This is what I get when I try to start a new Tiva-C LP project. When I go to 'Help'->'Install New Software', there's a TI Tiva-C device support and GCC Arm Tools Update site listed but nothing to add.
How do I get this working ?
Hehe, I don't remember but I do think so. Would they appear in the target list and related sites in the update list if not ?
oppa@oppa-hex-ssd:~/bin/ccsv6/ccsv6$ ls tools/compiler/ C5500_4.4.1 dmed gcc-arm-none-eabi-4_7-2012q4 MSP430_4.2.2 oppa@oppa-hex-ssd:~/bin/ccsv6/ccsv6$ ls tools/compiler/gcc-arm-none-eabi-4_7-2012q4/ arm-none-eabi bin lib share oppa@oppa-hex-ssd:~/bin/ccsv6/ccsv6$
This is from /home/oppa/bin/ccsv6/ccsv6/install_logs/ccs_setup_6.0.0.00091_install.log
06/11/2014 16:13:27 - writeDebugFile - Edition selected: ::edition0 06/11/2014 16:13:27 - writeDebugFile - Product Families selected: 06/11/2014 16:13:27 - writeDebugFile - PF_MSP430 06/11/2014 16:13:27 - writeDebugFile - PF_C28 06/11/2014 16:13:27 - writeDebugFile - PF_STELLARIS 06/11/2014 16:13:27 - writeDebugFile - PF_SITARA 06/11/2014 16:13:27 - writeDebugFile - PF_OMAPL13 06/11/2014 16:13:27 - writeDebugFile - PF_C6000_SINGLE 06/11/2014 16:13:27 - writeDebugFile - PF_C6000_MULTI 06/11/2014 16:13:27 - writeDebugFile - Components to be installed: 06/11/2014 16:13:27 - writeDebugFile - MSP430_CGT_HELP 06/11/2014 16:13:27 - writeDebugFile - CGT_DEFAULTLIBS_MSP430 06/11/2014 16:13:27 - writeDebugFile - DMED 06/11/2014 16:13:27 - writeDebugFile - GCC_ARM_COMPILER 06/11/2014 16:13:27 - writeDebugFile - EMU_STELLARIS 06/11/2014 16:13:27 - writeDebugFile - TIVA_TM4C 06/11/2014 16:13:27 - writeDebugFile - TIVA_TM4E 06/11/2014 16:13:27 - writeDebugFile - DEV_SUPPORT_OMAP 06/11/2014 16:13:27 - writeDebugFile - DEV_SUPPORT_C55XX 06/11/2014 16:13:27 - writeDebugFile - C5500_CGT_HELP 06/11/2014 16:13:27 - writeDebugFile - CGT_DEFAULTLIBS_C5500 06/11/2014 16:13:27 - writeDebugFile - EMU_MSP430 06/11/2014 16:13:27 - writeDebugFile - JRE 06/11/2014 16:13:27 - writeDebugFile - ECLIPSE 06/11/2014 16:13:27 - writeDebugFile - ECLIPSECORE 06/11/2014 16:13:27 - writeDebugFile - P2TOOLS 06/11/2014 16:13:27 - writeDebugFile - GMF 06/11/2014 16:13:27 - writeDebugFile - IDE_MAIN 06/11/2014 16:13:27 - writeDebugFile - IDE_WORKFLOW 06/11/2014 16:13:27 - writeDebugFile - DVT_COMMON 06/11/2014 16:13:27 - writeDebugFile - DVT_UIA 06/11/2014 16:13:27 - writeDebugFile - DVT_VIA_CCS 06/11/2014 16:13:27 - writeDebugFile - XULRUNNER 06/11/2014 16:13:27 - writeDebugFile - INSTALLER 06/11/2014 16:13:27 - writeDebugFile - IDE_MSP430 06/11/2014 16:13:27 - writeDebugFile - DS 06/11/2014 16:13:27 - writeDebugFile - IDE_C2000 06/11/2014 16:13:27 - writeDebugFile - IDE_ARM 06/11/2014 16:13:27 - writeDebugFile - EMU_TI 06/11/2014 16:13:27 - writeDebugFile - EMU_C2000_FLASH 06/11/2014 16:13:27 - writeDebugFile - EMU_C2000 06/11/2014 16:13:27 - writeDebugFile - GREE_C2000_SUPPORT 06/11/2014 16:13:27 - writeDebugFile - DVT_TRACE 06/11/2014 16:13:27 - writeDebugFile - DEV_SUPPORT_SITARA 06/11/2014 16:13:27 - writeDebugFile - DEV_SUPPORT_SHARED 06/11/2014 16:13:27 - writeDebugFile - ARM_QT 06/11/2014 16:13:27 - writeDebugFile - IDE_C6000 06/11/2014 16:13:27 - writeDebugFile - IDE_C5500 06/11/2014 16:13:27 - writeDebugFile - EMU_TI_XDS100 06/11/2014 16:13:27 - writeDebugFile - EMU_TI_XDS200
One quick way to check is to re-run the installer and point it to the existing installation. It should allow you to add/remove components and show which are currently installed.
Hehe, it's complaining that the directory is not empty and crashes.
Invalid external http://software-dl.ti.com/ccs/esd/CCSv6/CCS6.0.0.00091_linux and internal http://go-bradley.am.dhcp.ti.com/CCS6.0.0.00091_linux urls Invalid external http://software-dl.ti.com/ccs/esd/CCSv6/CCS6.0.0.00091_linux and internal http://go-bradley.am.dhcp.ti.com/CCS6.0.0.00091_linux urls while executing "error "Invalid external $m_exturl and internal $m_inturl urls"" (object "::manifest0" method "::Manifest::setComponentLocation" body line 16) invoked from within "setComponentLocation $component " (object "::manifest0" method "::Manifest::readManifestFiles" body line 12) invoked from within "$_instance readManifestFiles" (procedure "::Manifest::instance" body line 6) invoked from within "Manifest::instance" (object "::iSAPane0" method "::BaseTreePane::createPane" body line 34) invoked from within "::iSAPane0 createPane" ("uplevel" body line 1) invoked from within "uplevel #0 [string map $map $command]" (procedure "_eval_command" line 22) invoked from within "_eval_command $path $cmd $item" (procedure "Wizard::createstep" line 29) invoked from within "Wizard::createstep $path $item" (procedure "Wizard::raise" line 20) invoked from within "Wizard::raise $path $item $generateEvent" (procedure "Wizard::next" line 24) invoked from within "Wizard::next .wizard 1" ("eval" body line 1) invoked from within "eval [linsert $args 0 Wizard::$cmd .wizard]" (procedure ".wizard" line 1) invoked from within ".wizard next 1" invoked from within ".wizard.buttons.b1:cmd invoke" ("uplevel" body line 1) invoked from within "uplevel #0 [list $path:cmd invoke]" (procedure "TTKButton::invoke" line 2) invoked from within "TTKButton::invoke .wizard.buttons.b1" ("eval" body line 1) invoked from within "eval [linsert $args 0 TTKButton::$cmd .wizard.buttons.b1]" (procedure ".wizard.buttons.b1" line 1) invoked from within ".wizard.buttons.b1 invoke " invoked from within ".wizard.buttons.b1:cmd instate {pressed !disabled} { .wizard.buttons.b1 state !pressed; .wizard.buttons.b1 invoke }" ("uplevel" body line 1) invoked from within "uplevel #0 [list $path:cmd instate] $args" (procedure "TTKButton::instate" line 2) invoked from within "TTKButton::instate .wizard.buttons.b1 {pressed !disabled} { .wizard.buttons.b1 state !pressed; .wizard.buttons.b1 invoke }" ("eval" body line 1) invoked from within "eval [linsert $args 0 TTKButton::$cmd .wizard.buttons.b1]" (procedure ".wizard.buttons.b1" line 1) invoked from within ".wizard.buttons.b1 instate {pressed !disabled} { .wizard.buttons.b1 state !pressed; .wizard.buttons.b1 invoke } " (command bound to event)
Stephan,
I noticed you are using a beta version of v6. i would recommend uninstalling that and installing the full release version (6.0.0.00190). Make sure you install Tiva support and the ARM compiler when doing so.
Thanks
ki
Hi,
downloaded and installed a fresh copy. It's pulling the 'ware's right now. Installer was complaining about a missing libudev.so.0. libudev is installed, a google search made me fool the installer by symlinking libudev.so.1. Looks good so far.
Well, there's still the old installation around. I will just delete the folder.
Thanks and have a nice weekend,
Stephan