Hi,
I have two questions about XDS100v1.
First of all, See below.
* XDS100v1's General features
- Support for “JTAG reset”/"wait-in-reset" boot-modes using the two EMU pins sampled by the nTRST pin.
- Support for “Power-on reset” boot-modes using the two EMU pins sampled by the TVD pin.
- Support for the configuration of the EMU pin features through Code Composer Studio™ Setup “connection properties” dialogs similar to those for the XDS560 Rev-D cable.
- Support for “target power-loss detection” via the TVD pin even when Code Composer Studio™ is not running, and applying boot-modes at Code Composer Studio™ start-up.
etc...
* XDS100v1's Own features
- Support for the following processors cores : TMS320C28x, TMS320C54x, TMS320C55x, TMS320C64x+, and TMS320C674x.
etc...
What is the functionality excluded if removed EMU0, EMU1 pins on XDS100v1.
In that case, Which processors cores does it support ?