This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
at the moment we are using mainly IAR Embedded workbench and now want to additionaly support CCE/CCS builds of our projects.
Our directory structure (which we don't want to change) hast several projects, that rely on a lot of common files (headers, c-source-files) which are maintained centrally outside the customer-specific files in the project directories.
Example structure with directories "includes/" and "common_sources/" outside the project directories.
|
|->project_1/
| |->src/
| |->project-files
|->project_2/
| |->src/
| |->project-files
|->includes/
| |->headerfile_1.h
| |->headerfile_2.h
|->common_sources/
|->sourcefile_1.c
|->sourcefile_2.c
How do I tell Code Composer for e.g. project_1 that it should also compile sourcefile_1.c?
In IAR I can use "Add files" which includes the files relative to the project directory in the form "../common_sources/sourcefile_1.c".
I tried to use "Project->Link Files to Active Project..." in CCE to do this, but this adds the absolute path to the files, not the relative path as I need it.
Because of this the build isn't working any more when the project structure is moved to a different location, e.g. during a checkout to a different directory or machine out of our versioning sytem.
I didn't have the possibility to try CCS up to now, so I am also very interested how its behaviour is.
For the include directories I use the Eclipse macro ${project_loc} to reference relative to the project path. For the above example this would be:
"${project_loc}/../include"
Does anybody know how to reference the source files relative to the project directory in CCE and CCS?
I hope there is a way to do this, as I regard this as pretty essential for a multi-build/multi-user enviroment...
Hello Horst,
CCE does not allow to use relative paths. Linked Path variables can be used to refer to source files existing outside projects directory structure. CCE requires end user to define linked resource variables. CCSv4, which can also be used for MSP430 development, has a feature that allows to automatically define these variables during project import through macros.ini file. see link below for more information on linked resource variables. The topic is written for CCS v4, but majority of it is applicable to CCE as well, except automated definition of linked path variables through macros.ini