This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv4 crashes when program is loaded the second time.



My setup was working fine for many weeks, then for some reason CCCSv4 is creashing when I load a program the second time.

This problem is not specific to the program that I am running.

If I reopen CCSv4 without power cycling the board I see errors either when trying to connect to dsp or when loading the program.

Version: 4.0.0.15002

Emulator: xds510usb

Board: DSK DA830

BIOS version: 6.20.01.41

XDCTools: 3.15.02.62

I have attached the dump file and exe.