This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123

Hi everyone,

I was writing a code for usual 16x2 LCD with TM4C123 microcontroller and i was getting the following error message:

.\LCD.axf: Error: L6221E: Execution region ER_RO with Execution range [0x00000000,0x00000608) overlaps with Execution region ER_ZI with Execution range [0x00000000,0x00000460).

Can any please assist me to figure out what the problem is with the code?

Attacheds are my codes:

.

// LCD.c
// Runs on LM3S1968
// Simple device driver for the LCD
// Valvano
// August 2, 2011

/* This example accompanies the book
   "Embedded Systems: Real Time Interfacing to the Arm Cortex M3",
   ISBN: 978-1463590154, Jonathan Valvano, copyright (c) 2011

   Section 4.7.1, Program 4.2 and Program 4.3

 Copyright 2011 by Jonathan W. Valvano, valvano@mail.utexas.edu
    You may use, edit, run or distribute this file
    as long as the above copyright notice remains
 THIS SOFTWARE IS PROVIDED "AS IS".  NO WARRANTIES, WHETHER EXPRESS, IMPLIED
 OR STATUTORY, INCLUDING, BUT NOT LIMITED TO, IMPLIED WARRANTIES OF
 MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE.
 VALVANO SHALL NOT, IN ANY CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL,
 OR CONSEQUENTIAL DAMAGES, FOR ANY REASON WHATSOEVER.
 For more information about my classes, my research, and my books, see
 http://users.ece.utexas.edu/~valvano/
 */

/*
  size is 1*8
  if do not need to read busy, then you can tie R/W=ground
  ground = pin 1    Vss
  power  = pin 2    Vdd   +3.3V or +5V depending on the device
  ground = pin 3    Vlc   grounded for highest contrast
  PA0    = pin 4    RS    (1 for data, 0 for control/status)
  PA1    = pin 5    R/W   (1 for read, 0 for write)
  PA2    = pin 6    E     (enable)
  PF0    = pin 7    DB0   (8-bit data)
  PF1    = pin 8    DB1
  PF2    = pin 9    DB2
  PF3    = pin 10   DB3
  PF4    = pin 11   DB4
  PF5    = pin 12   DB5
  PF6    = pin 13   DB6
  PF7    = pin 14   DB7
8 characters are configured as 1 rows of 8
addr  00 01 02 03 04 05 06 07
*/
//#include "LCD.h"
#include "tm4c123gh6pm.h"
#include "systick.h"

#define E  4 // on PA2
#define RW 2 // on PA1
#define RS 1 // on PA0
#define LCDDATA (*((volatile unsigned long *)0x400253FC))   // PORTF
#define LCDCMD (*((volatile unsigned long *)0x4000401C))    // PA2-PA0
#define BusFreq 50            // assuming a 50 MHz bus clock
#define T6us 6*BusFreq        // 6us
#define T40us 40*BusFreq      // 40us
#define T160us 160*BusFreq    // 160us
#define T1600us 1600*BusFreq  // 1.60ms
#define T5ms 5000*BusFreq     // 5ms#define T15ms 15000*BusFreq   // 15ms
void OutCmd(unsigned char command){
  LCDDATA = command;
  LCDCMD = 0;           // E=0, R/W=0, RS=0
  SysTick_Wait(T6us);   // wait 6us
  LCDCMD = E;           // E=1, R/W=0, RS=0
  SysTick_Wait(T6us);   // wait 6us
  LCDCMD = 0;           // E=0, R/W=0, RS=0
  SysTick_Wait(T40us);  // wait 40us
}

// Initialize LCD
// Inputs: none
// Outputs: none
void LCD_Init(void){ volatile long delay;
  SYSCTL_RCGC2_R |= 0x00000021;  // 1) activate clock for Ports F and A
  delay = SYSCTL_RCGC2_R;        // allow time for clock to start
  GPIO_PORTF_DIR_R = 0xFF;       // 2) set direction register
  GPIO_PORTA_DIR_R |= 0x07;
  GPIO_PORTF_AFSEL_R = 0x00;     // 3) regular port function
  GPIO_PORTA_AFSEL_R &= ~0x07;
  GPIO_PORTF_DEN_R = 0xFF;       // 4) enable digital 
	
  GPIO_PORTA_DEN_R |= 0x07;
  GPIO_PORTF_DR8R_R = 0xFF;      // 5) enable 8 mA drive
  GPIO_PORTA_DR8R_R |= 0x07;
  SysTick_Init();       // Program 2.10
  LCDCMD = 0;           // E=0, R/W=0, RS=0
  SysTick_Wait(T5ms);  // Wait >15 ms after power is applied
  OutCmd(0x30);         // command 0x30 = Wake up
  SysTick_Wait(T5ms);   // must wait 5ms, busy flag not available
  OutCmd(0x30);         // command 0x30 = Wake up #2
  SysTick_Wait(T160us); // must wait 160us, busy flag not available
  OutCmd(0x30);         // command 0x30 = Wake up #3
  SysTick_Wait(T160us); // must wait 160us, busy flag not available
  OutCmd(0x38);         // Function set: 8-bit/2-line
  OutCmd(0x10);         // Set cursor
  OutCmd(0x0c);         // Display ON; Cursor ON
  OutCmd(0x06);         // Entry mode set
}
// Output a character to the LCD
// Inputs: letter is ASCII character, 0 to 0x7F
// Outputs: none
void LCD_OutChar(unsigned char letter){
  LCDDATA = letter;
  LCDCMD = RS;          // E=0, R/W=0, RS=1
  SysTick_Wait(T6us);   // wait 6us
  LCDCMD = E+RS;        // E=1, R/W=0, RS=1
  SysTick_Wait(T6us);   // wait 6us
  LCDCMD = RS;          // E=0, R/W=0, RS=1
  SysTick_Wait(T40us);  // wait 40us
}

// Clear the LCD
// Inputs: none
// Outputs: none
void LCD_Clear(void){
  OutCmd(0x01);          // Clear Display
  SysTick_Wait(T1600us); // wait 1.6ms
  OutCmd(0x02);          // Cursor to home
  SysTick_Wait(T1600us); // wait 1.6ms
}

//------------LCD_OutString------------
// Output String (NULL termination)
// Input: pointer to a NULL-terminated string to be transferred
// Output: none
void LCD_OutString(char *pt){
  while(*pt){
    LCD_OutChar(*pt);
    pt++;
  }
}

//-----------------------LCD_OutUDec-----------------------
// Output a 32-bit number in unsigned decimal format
// Input: 32-bit number to be transferred
// Output: none
// Variable format 1-10 digits with no space before or after
void LCD_OutUDec(unsigned long n){
// This function uses recursion to convert decimal number
//   of unspecified length as an ASCII string
  if(n >= 10){
    LCD_OutUDec(n/10);
    n = n%10;
  }
  LCD_OutChar(n+'0'); /* n is between 0 and 9 */
}

//--------------------------LCD_OutUHex----------------------------
// Output a 32-bit number in unsigned hexadecimal format
// Input: 32-bit number to be transferred
// Output: none
// Variable format 1 to 8 digits with no space before or after
void LCD_OutUHex(unsigned long number){
// This function uses recursion to convert the number of
//   unspecified length as an ASCII string
  if(number >= 0x10){
    LCD_OutUHex(number/0x10);
    LCD_OutUHex(number%0x10);
  }
  else{
    if(number < 0xA){
      LCD_OutChar(number+'0');
     }
    else{
      LCD_OutChar((number-0x0A)+'A');
    }
  }
}

int main (void)
{
//LCD_Init();
//SysTick_Init();

//	while(1);
}
// SysTick.c
// Runs on LM4F120/TM4C123
// Provide functions that initialize the SysTick module, wait at least a
// designated number of clock cycles, and wait approximately a multiple
// of 10 milliseconds using busy wait.  After a power-on-reset, the
// LM4F120 gets its clock from the 16 MHz precision internal oscillator,
// which can vary by +/- 1% at room temperature and +/- 3% across all
// temperature ranges.  If you are using this module, you may need more
// precise timing, so it is assumed that you are using the PLL to set
// the system clock to 50 MHz.  This matters for the function
// SysTick_Wait10ms(), which will wait longer than 10 ms if the clock is
// slower.
// Daniel Valvano
// September 11, 2013

/* This example accompanies the books
   "Embedded Systems: Introduction to ARM Cortex M Microcontrollers",
   ISBN: 978-1469998749, Jonathan Valvano, copyright (c) 2013
   Volume 1, Program 4.7
   
   "Embedded Systems: Real Time Interfacing to ARM Cortex M Microcontrollers",
   ISBN: 978-1463590154, Jonathan Valvano, copyright (c) 2013
   Program 2.11, Section 2.6

 Copyright 2013 by Jonathan W. Valvano, valvano@mail.utexas.edu
    You may use, edit, run or distribute this file
    as long as the above copyright notice remains
 THIS SOFTWARE IS PROVIDED "AS IS".  NO WARRANTIES, WHETHER EXPRESS, IMPLIED
 OR STATUTORY, INCLUDING, BUT NOT LIMITED TO, IMPLIED WARRANTIES OF
 MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE.
 VALVANO SHALL NOT, IN ANY CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL,
 OR CONSEQUENTIAL DAMAGES, FOR ANY REASON WHATSOEVER.
 For more information about my classes, my research, and my books, see
 http://users.ece.utexas.edu/~valvano/
 */

#define NVIC_ST_CTRL_R          (*((volatile unsigned long *)0xE000E010))
#define NVIC_ST_RELOAD_R        (*((volatile unsigned long *)0xE000E014))
#define NVIC_ST_CURRENT_R       (*((volatile unsigned long *)0xE000E018))
#define NVIC_ST_CTRL_COUNT      0x00010000  // Count flag
#define NVIC_ST_CTRL_CLK_SRC    0x00000004  // Clock Source
#define NVIC_ST_CTRL_INTEN      0x00000002  // Interrupt enable
#define NVIC_ST_CTRL_ENABLE     0x00000001  // Counter mode
#define NVIC_ST_RELOAD_M        0x00FFFFFF  // Counter load value

// Initialize SysTick with busy wait running at bus clock.
void SysTick_Init(void){
  NVIC_ST_CTRL_R = 0;                   // disable SysTick during setup
  NVIC_ST_RELOAD_R = NVIC_ST_RELOAD_M;  // maximum reload value
  NVIC_ST_CURRENT_R = 0;                // any write to current clears it
                                        // enable SysTick with core clock
  NVIC_ST_CTRL_R = NVIC_ST_CTRL_ENABLE+NVIC_ST_CTRL_CLK_SRC;
}
// Time delay using busy wait.
// The delay parameter is in units of the core clock. (units of 20 nsec for 50 MHz clock)
void SysTick_Wait(unsigned long delay){
  volatile unsigned long elapsedTime;
  unsigned long startTime = NVIC_ST_CURRENT_R;
  do{
    elapsedTime = (startTime-NVIC_ST_CURRENT_R)&0x00FFFFFF;
  }
  while(elapsedTime <= delay);
}
// Time delay using busy wait.
// This assumes 50 MHz system clock.
void SysTick_Wait10ms(unsigned long delay){
  unsigned long i;
  for(i=0; i<delay; i++){
    SysTick_Wait(500000);  // wait 10ms (assumes 50 MHz clock)
  }
}

Thanks in advance.

Regards.