This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

convert .out to srec file

Hi,

I convert .out file to S2 using Hex500. However, I found the address of one recorder is not continuous. see address 884 below.

           S222 000865 00000000000000000000000000000000000000000000000000000000000070

           S222 000874 00000000000000000000000000000000000000000000000000000000000061

          S222 000884 D1F4F495000000000000000000000000000000000000000000000000000003

           S222 000893 00000000000000000000000000000000000000000000000000000000000042

           S222 0008A2 00000000000000000000000000000000000000000000000000000000000033

it suppose to be 000883 instead of 000884. here one word is skipped. Is this normal or something went wrong?

Any help is appreciated!

Ron