Hi,
I have one question regarding the cofffile download using the host processor. i saw in the spec spraa08-April2009 on page 6.it specifies the bits 8 to 11 of section header flags are used for defining the alignment, and after taking pow(2, bits(8-11)), you get the alignment.so, as i understand that í have to add this alignment(assumed in bytes,because its not clearly specified) to the physical address of the DSP ? has some one done this already before as i don't know if this really works or not ?
Thanks for your help,