Because I believe this a Code Composer component issue, I've started asking here. I'm trying to build ethernetip_adapter example in "C:\ti\am335x_sysbios_ind_sdk_1.1.0.4\sdk\examples\ethernetip_adapter". This example uses NDK, so I've based my requirements on the NDK version.
The project is imported correctly but fails to build with the error below. The only thing I am not sure about is the Code Generation Tools version. The release notes on the NDK say it should be "Code Generation Tools 5.0.1 (Application Build)", but where would I check this version?
Thanks,
John C.
**** Build of configuration Debug for project ethernetip_adapter ****
"C:\\ti\\ccsv5_5\\ccsv5\\utils\\bin\\gmake" -k all
'Building file: ../app.cfg'
'Invoking: XDCtools'
"C:/ti/xdctools_3_25_04_88/xs" --xdcpath="C:/ti/ccsv5_5/ccsv5/ccs_base;C:/ti/bios_6_40_01_15/packages;C:/ti/ndk_2_23_02_03/packages;C:/ti/ccsv5_5/xdais_7_21_01_07/packages;C:/ti/ccsv5_5/xdais_7_21_01_07/examples;C:/ti/nsp_1_10_02_09/packages;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.A8Fnv -p ti.platforms.evmAM3359 -r debug -c "C:/ti/ccsv5_5/ccsv5/tools/compiler/arm_5.1.6" --compileOptions "-g --optimize_with_debug" "../app.cfg"
making package.mak (because of package.bld) ...
generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...
configuring app.xea8fnv from package/cfg/app_pea8fnv.cfg ...
generating custom ti.sysbios library makefile ...
js: "C:/ti/bios_6_40_01_15/packages/ti/sysbios/Build.xs", line 1313: Error: template generation of 'C:\Users\jc\workspace_v5_5\ethernetip_adapter/src/sysbios/makefile' failed: InternalError: XDC runtime error: ti.sysbios.family.arm.IntrinsicsSupport/common$: no property named 'outPolicy'
"C:/ti/bios_6_40_01_15/packages/ti/sysbios/makefile.xdt#143(eval)", line 1
"C:/ti/bios_6_40_01_15/packages/ti/sysbios/makefile.xdt", line 143
"C:/ti/bios_6_40_01_15/packages/ti/sysbios/makefile.xdt", line 192
"C:/ti/bios_6_40_01_15/packages/ti/sysbios/Build.xdt", line 69
"C:/ti/bios_6_40_01_15/packages/ti/sysbios/Build.xdt", line 79
gmake.exe: *** [package/cfg/app_pea8fnv.xdl] Error 1
js: "C:/ti/xdctools_3_25_04_88/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
making ../src/sysbios/sysbios.aea8fnv ...
gmake[1]: Entering directory `C:/Users/jc/workspace_v5_5/ethernetip_adapter/src/sysbios'
clea8fnv C:/ti/ccsv5_5/bios_6_35_04_50/packages/ti/sysbios/BIOS.c ...
asmea8fnv C:/ti/ccsv5_5/bios_6_35_04_50/packages/ti/sysbios/family/arm/IntrinsicsSupport_asm.asm ...
asmea8fnv C:/ti/ccsv5_5/bios_6_35_04_50/packages/ti/sysbios/family/arm/TaskSupport_asm.asm ...
asmea8fnv C:/ti/ccsv5_5/bios_6_35_04_50/packages/ti/sysbios/family/arm/exc/Exception_asm.asm ...
asmea8fnv C:/ti/ccsv5_5/bios_6_35_04_50/packages/ti/sysbios/family/arm/a8/TimestampProvider_asm.asm ...
asmea8fnv C:/ti/ccsv5_5/bios_6_35_04_50/packages/ti/sysbios/family/arm/a8/Mmu_asm.asm ...
asmea8fnv C:/ti/ccsv5_5/bios_6_35_04_50/packages/ti/sysbios/family/arm/a8/Cache_asm.asm ...
asmea8fnv C:/ti/ccsv5_5/bios_6_35_04_50/packages/ti/sysbios/family/arm/a8/intcps/Hwi_asm.s470 ...
asmea8fnv C:/ti/ccsv5_5/bios_6_35_04_50/packages/ti/sysbios/family/arm/a8/intcps/Hwi_asm_switch.s470 ...
asmea8fnv C:/ti/ccsv5_5/bios_6_35_04_50/packages/ti/sysbios/timers/gptimer/Timer_asm.s470 ...
asmea8fnv C:/ti/ccsv5_5/bios_6_35_04_50/packages/ti/sysbios/timers/dmtimer/Timer_asm.s470 ...
area8fnv BIOS.obj arm_IntrinsicsSupport_asm.obj arm_TaskSupport_asm.obj exc_Exception_asm.obj a8_TimestampProvider_asm.obj a8_Mmu_asm.obj a8_Cache_asm.obj intcps_Hwi_asm.obj intcps_Hwi_asm_switch.obj gptimer_Timer_asm.obj dmtimer_Timer_asm.obj ...
gmake[1]: Leaving directory `C:/Users/jc/workspace_v5_5/ethernetip_adapter/src/sysbios'
gmake: *** No rule to make target `C:/Users/jc/protocols/ethernetip_adapter/drivers/icss_dlr.c', needed by `icss_dlr.obj'.
gmake: *** No rule to make target `C:/Users/jc/protocols/ethernetip_adapter/drivers/icss_eip_driver.c', needed by `icss_eip_driver.obj'.
gmake: Target `all' not remade because of errors.
**** Build Finished ****