This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Target Configuration for Jacinto6

Hi,

At CCS5.2, I am trying to create a target configuration file for Jacinto6 (c66 dsp),

there is no device to correspond jacinto6 at "board or device" in the configuration file "TargetConfiguration.ccxml"
,such as "OMAP5" or "DRA7x".

What should be set in the "board or device" configuration?

Do I need something installed?

Or Do I need and upgrade of CCS?

my environment is follows.

CCS:Version: 5.2.1.00018
JTAG : Spectrum Degital XDS560v2stm

Thanks.

  • Hi Naoto,

    Or Do I need and upgrade of CCS?

    Yes, you need to upgrade your CCS probably to CCS v6. Upgrading your current to CCS v5.5 should also do the trick by going to Help -> Check for updates

    Regards,

    Gautam