This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Crash Dump Analysis as a library?

Hi,

Following the instructions from http://processors.wiki.ti.com/index.php/Crash_Dump_Analysis one can do offline analysis of an exception on e.g. C67 processor.

But as I understand, to use it, one needs to have CCS installed.

Is there any library that allows to at least extract the call stack from memory dumped during crash that does not require CCS installed?

Wojtek

  • Hello Wojtek,

    The analysis leverages many components of the CCS debug engine so you would need an installation of CCS for this. There is no smaller standalone library or component that you can use in place of an installation of CCS. Sorry.

    ki