Hi,
When I start to run the target, e.g. debugsession.target.run(), it tells the following messages. What does it mean, "This is not a valid vbusp cfg address : 0x00033080"?
Br,
run: ENTRY run: Requesting target run waitUntil: ENTRY flag: onRunning timeout: 150000 (ms) onEvent: Target is now running waitUntil: RETURN true run: Target is running, waiting for a halt waitUntil: ENTRY flag: onHalt timeout: 150000 (ms) Simulator config cpu 2 : Startup pre started. System.FARADAY.SHARED_SYSTEM.USER5 : AI Reset interface - end System.FARADAY.SHARED_SYSTEM.USER6 : Reset System.FARADAY.SHARED_SYSTEM.USER1 : Init Done This is not a valid vbusp cfg address : 0x00033080 This is not a valid vbusp cfg address : 0x00033080 This is not a valid vbusp cfg address : 0x00030008 This is not a valid vbusp cfg address : 0x0003000c This is not a valid vbusp cfg address : 0x00030028 This is not a valid vbusp cfg address : 0x0003002c This is not a valid vbusp cfg address : 0x00030808 This is not a valid vbusp cfg address : 0x0003080c This is not a valid vbusp cfg address : 0x00030828 This is not a valid vbusp cfg address : 0x0003082c This is not a valid vbusp cfg address : 0x00031008 This is not a valid vbusp cfg address : 0x0003100c This is not a valid vbusp cfg address : 0x00031028 This is not a valid vbusp cfg address : 0x0003102c This is not a valid vbusp cfg address : 0x00031808 This is not a valid vbusp cfg address : 0x0003180c This is not a valid vbusp cfg address : 0x00031828 This is not a valid vbusp cfg address : 0x0003182c This is not a valid vbusp cfg address : 0x00032008 This is not a valid vbusp cfg address : 0x0003200c This is not a valid vbusp cfg address : 0x00032028 This is not a valid vbusp cfg address : 0x0003202c This is not a valid vbusp cfg address : 0x00032808 This is not a valid vbusp cfg address : 0x0003280c This is not a valid vbusp cfg address : 0x00032828 This is not a valid vbusp cfg address : 0x0003282c This is not a valid vbusp cfg address : 0x00033104 This is not a valid vbusp cfg address : 0x00033124 Simulator config cpu 2 : Startup post started. Simulator config cpu 2 : Platform ready ind sent.